| Interface | Description | 
|---|---|
| FeatureSelection | |
| MoveJMotionParameters | |
| MoveJMoveNodeConfig | |
| MoveLMotionParameters | |
| MoveLMoveNodeConfig | |
| MoveNodeConfig | |
| MoveNodeConfigFactory | Deprecated
 Use the configuration builders available in  
MoveNodeConfigBuilders interface which is accessible
 through MoveNode.getConfigBuilders(). | 
| MoveNodeFeature | |
| MoveNodeTCP | |
| MovePMotionParameters | |
| MovePMoveNodeConfig | |
| TCPSelection | |
| TCPSelectionFactory | 
 This interface supplies methods for creating TCP selections for a Move node configuration. 
 | 
| Enum | Description | 
|---|---|
| FeatureSelection.SelectionType | |
| MoveNodeConfig.ConfigType | 
 The configuration type used to determine which type of configuration this instance is. 
 | 
| TCPSelection.SelectionType | 
Copyright © 2020. All rights reserved.