public interface MoveNode extends ProgramNode
| Modifier and Type | Method and Description | 
|---|---|
MoveNodeConfig | 
getConfig()  | 
MoveNodeConfigBuilders | 
getConfigBuilders()
This method returns a  
MoveNodeConfigBuilders to build configurations for this node type. | 
MoveNodeConfigFactory | 
getConfigFactory()
Deprecated. 
 
Use  
getConfigBuilders() instead. | 
TCPSelectionFactory | 
getTCPSelectionFactory()
This method returns a  
TCPSelectionFactory to create a TCP selection. | 
MoveNode | 
setConfig(MoveNodeConfig config)
Set a configuration on this node. 
 | 
@Deprecated MoveNodeConfigFactory getConfigFactory()
getConfigBuilders() instead.MoveNode setConfig(MoveNodeConfig config)
config - the configuration to be set.IllegalArgumentException - if this node is a MoveP containing one or more CircleMoveNode and the node
 configuration is attempted to be changed to MoveJ or MoveL. CircleMoveNode is only allowed under a MoveP.
 All instances of CircleMoveNode need to be deleted before the configuration can be changed from a MoveP to
 MoveJ or MoveL.IllegalArgumentException - if this node is a MoveL or MoveP containing one or more DirectionNode and
 the node configuration is attempted to be changed to a MoveJ.
 DirectionNode is only allowed under a MoveL or MoveP. All instances of DirectionNode need to be
 deleted before the configuration can be changed from a MoveL or MoveP to a MoveJ.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
 scope (see also UndoRedoManager).MoveNodeConfig getConfig()
MoveNodeConfigBuilders getConfigBuilders()
MoveNodeConfigBuilders to build configurations for this node type.TCPSelectionFactory getTCPSelectionFactory()
TCPSelectionFactory to create a TCP selection.Copyright © 2020. All rights reserved.