public static enum MoveNodeConfig.ConfigType extends Enum<MoveNodeConfig.ConfigType>
Enum Constant and Description |
---|
MOVE_J
Movement type is MoveJ.
|
MOVE_L
Movement type is MoveL.
|
MOVE_P
Movement type is MoveP.
|
Modifier and Type | Method and Description |
---|---|
static MoveNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static MoveNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final MoveNodeConfig.ConfigType MOVE_J
Movement type is MoveJ.
The config instance can be cast toMoveJMoveNodeConfig
.public static final MoveNodeConfig.ConfigType MOVE_L
Movement type is MoveL.
The config instance can be cast toMoveLMoveNodeConfig
.public static final MoveNodeConfig.ConfigType MOVE_P
Movement type is MoveP.
The config instance can be cast toMovePMoveNodeConfig
.public static MoveNodeConfig.ConfigType[] values()
for (MoveNodeConfig.ConfigType c : MoveNodeConfig.ConfigType.values()) System.out.println(c);
public static MoveNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.