public static enum FeatureSelection.SelectionType extends Enum<FeatureSelection.SelectionType>
Enum Constant and Description |
---|
FEATURE
Feature is selected.
|
UNRESOLVED_FEATURE
The selected feature is no longer available (e.g.
|
Modifier and Type | Method and Description |
---|---|
static FeatureSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static FeatureSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final FeatureSelection.SelectionType UNRESOLVED_FEATURE
public static final FeatureSelection.SelectionType FEATURE
Feature is selected.
The Selection instance can be cast toMoveNodeFeature
.public static FeatureSelection.SelectionType[] values()
for (FeatureSelection.SelectionType c : FeatureSelection.SelectionType.values()) System.out.println(c);
public static FeatureSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.