| Interface | Description | 
|---|---|
| AnalogInputDomainConfig | 
 
 This interface represents the analog input domain configuration for the two analog inputs in the Tool I/O Interface. 
 | 
| AnalogInputModeConfig | 
 This interface represents a configuration of the analog inputs in the Tool I/O Interface. 
 | 
| CommunicationInterfaceConfig | 
 
 This interface represents the Tool Communication Interface (TCI) configuration for the two analog inputs in the Tool
 I/O Interface. 
 | 
| DigitalOutputModeConfig | 
 This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface. 
 | 
| StandardDigitalOutputModeConfig | 
 
 This interface represents the digital output mode configuration for the digital outputs in the Tool I/O Interface. 
 | 
| ToolIOInterface | 
 This interface allows for querying the settings of the Tool I/O Interface 
 | 
| Enum | Description | 
|---|---|
| AnalogInputDomainConfig.AnalogDomain | 
 The type of the electrical domain used by the analog inputs in the connector in the robot tool 
 | 
| AnalogInputModeConfig.ConfigType | 
 The configuration type used to determine which type of configuration this instance is. 
 | 
| CommunicationInterfaceConfig.BaudRate | 
 Available options for the baud rate used for communication 
 | 
| CommunicationInterfaceConfig.Parity | 
 Available options for the parity used for communication 
 | 
| CommunicationInterfaceConfig.StopBits | 
 Available options for the number of stop bits used for communication 
 | 
| DigitalOutputModeConfig.ConfigType | 
 The configuration type used to determine which type of configuration this instance is. 
 | 
| StandardDigitalOutputModeConfig.OutputMode | 
 Available output modes for the digital outputs in the connector in the robot tool 
 | 
| ToolIOInterface.OutputVoltage | 
 Available options for the output voltage level for the power supply that delivers power to the connector in the
 robot tool 
 | 
Copyright © 2019. All rights reserved.