public static enum CommunicationInterfaceConfig.BaudRate extends Enum<CommunicationInterfaceConfig.BaudRate>
| Enum Constant and Description | 
|---|
BAUD_115200  | 
BAUD_19200  | 
BAUD_1M  | 
BAUD_2M  | 
BAUD_38400  | 
BAUD_57600  | 
BAUD_5M  | 
BAUD_9600  | 
| Modifier and Type | Method and Description | 
|---|---|
static CommunicationInterfaceConfig.BaudRate | 
valueOf(String name)
Returns the enum constant of this type with the specified name. 
 | 
static CommunicationInterfaceConfig.BaudRate[] | 
values()
Returns an array containing the constants of this enum type, in
the order they are declared. 
 | 
public static final CommunicationInterfaceConfig.BaudRate BAUD_9600
public static final CommunicationInterfaceConfig.BaudRate BAUD_19200
public static final CommunicationInterfaceConfig.BaudRate BAUD_38400
public static final CommunicationInterfaceConfig.BaudRate BAUD_57600
public static final CommunicationInterfaceConfig.BaudRate BAUD_115200
public static final CommunicationInterfaceConfig.BaudRate BAUD_1M
public static final CommunicationInterfaceConfig.BaudRate BAUD_2M
public static final CommunicationInterfaceConfig.BaudRate BAUD_5M
public static CommunicationInterfaceConfig.BaudRate[] values()
for (CommunicationInterfaceConfig.BaudRate c : CommunicationInterfaceConfig.BaudRate.values()) System.out.println(c);
public static CommunicationInterfaceConfig.BaudRate valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2019. All rights reserved.