public interface ToolIOInterface
| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
ToolIOInterface.OutputVoltage
Available options for the output voltage level for the power supply that delivers power to the connector in the
 robot tool 
 | 
| Modifier and Type | Method and Description | 
|---|---|
AnalogInputModeConfig | 
getAnalogInputModeConfig()  | 
DigitalOutputModeConfig | 
getDigitalOutputModeConfig()  | 
ToolIOInterface.OutputVoltage | 
getOutputVoltage()  | 
ToolIOInterface.OutputVoltage getOutputVoltage()
@RequiredCapability(value=DIGITAL_OUTPUT_MODE) DigitalOutputModeConfig getDigitalOutputModeConfig()
CapabilityNotSupportedException - if the digital output mode capability is not available on the system.
 Use CapabilityManager.hasCapability(Capability) with ToolIOCapability.DIGITAL_OUTPUT_MODE to
 verify the availability.AnalogInputModeConfig getAnalogInputModeConfig()
Copyright © 2019. All rights reserved.