| Interface | Description | 
|---|---|
| AnalogInputModeConfigFactory | 
 Factory for creating configurations of the analog input mode for the analog inputs in the connector in the robot tool. 
 | 
| DigitalOutputModeConfigFactory | 
 
 Factory for creating configurations of the digital output mode for the digital outputs in the connector in the robot
 tool. 
 | 
| ToolIOInterfaceControlEvent | 
 This interface holds information relevant to the  
ToolIOInterfaceController.onControlGranted(ToolIOInterfaceControlEvent)
 and ToolIOInterfaceController.onControlToBeRevoked(ToolIOInterfaceControlEvent) events that occur when
 the control of the Tool I/O Interface resource has been assigned to a URCap or when the control is about to be revoked,
 respectively. | 
| ToolIOInterfaceControllable | 
 This is an interface for controlling/configuring the settings of the Tool I/O Interface 
 | 
| ToolIOInterfaceController | 
 
 This interface can be implemented to request control of the Tool I/O Interface. 
 | 
Copyright © 2019. All rights reserved.