| Class and Description | 
|---|
| ToolIOInterface
 This interface allows for querying the settings of the Tool I/O Interface 
 | 
| Class and Description | 
|---|
| AnalogInputDomainConfig.AnalogDomain
 The type of the electrical domain used by the analog inputs in the connector in the robot tool 
 | 
| AnalogInputModeConfig
 This interface represents a configuration of the analog inputs in the Tool I/O Interface. 
 | 
| AnalogInputModeConfig.ConfigType
 The configuration type used to determine which type of configuration this instance is. 
 | 
| CommunicationInterfaceConfig.BaudRate
 Available options for the baud rate used for communication 
 | 
| CommunicationInterfaceConfig.Parity
 Available options for the parity used for communication 
 | 
| CommunicationInterfaceConfig.StopBits
 Available options for the number of stop bits used for communication 
 | 
| DigitalOutputModeConfig
 This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface. 
 | 
| DigitalOutputModeConfig.ConfigType
 The configuration type used to determine which type of configuration this instance is. 
 | 
| StandardDigitalOutputModeConfig.OutputMode
 Available output modes for the digital outputs in the connector in the robot tool 
 | 
| ToolIOInterface.OutputVoltage
 Available options for the output voltage level for the power supply that delivers power to the connector in the
 robot tool 
 | 
| Class and Description | 
|---|
| AnalogInputDomainConfig
 
 This interface represents the analog input domain configuration for the two analog inputs in the Tool I/O Interface. 
 | 
| AnalogInputDomainConfig.AnalogDomain
 The type of the electrical domain used by the analog inputs in the connector in the robot tool 
 | 
| AnalogInputModeConfig
 This interface represents a configuration of the analog inputs in the Tool I/O Interface. 
 | 
| CommunicationInterfaceConfig
 
 This interface represents the Tool Communication Interface (TCI) configuration for the two analog inputs in the Tool
 I/O Interface. 
 | 
| CommunicationInterfaceConfig.BaudRate
 Available options for the baud rate used for communication 
 | 
| CommunicationInterfaceConfig.Parity
 Available options for the parity used for communication 
 | 
| CommunicationInterfaceConfig.StopBits
 Available options for the number of stop bits used for communication 
 | 
| DigitalOutputModeConfig
 This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface. 
 | 
| StandardDigitalOutputModeConfig
 
 This interface represents the digital output mode configuration for the digital outputs in the Tool I/O Interface. 
 | 
| StandardDigitalOutputModeConfig.OutputMode
 Available output modes for the digital outputs in the connector in the robot tool 
 | 
| ToolIOInterface
 This interface allows for querying the settings of the Tool I/O Interface 
 | 
| ToolIOInterface.OutputVoltage
 Available options for the output voltage level for the power supply that delivers power to the connector in the
 robot tool 
 | 
Copyright © 2019. All rights reserved.