public static enum AnalogInputDomainConfig.AnalogDomain extends Enum<AnalogInputDomainConfig.AnalogDomain>
| Enum Constant and Description | 
|---|
CURRENT
Analog input configured for electric current. 
 | 
VOLTAGE
Analog input configured for voltage. 
 | 
| Modifier and Type | Method and Description | 
|---|---|
static AnalogInputDomainConfig.AnalogDomain | 
valueOf(String name)
Returns the enum constant of this type with the specified name. 
 | 
static AnalogInputDomainConfig.AnalogDomain[] | 
values()
Returns an array containing the constants of this enum type, in
the order they are declared. 
 | 
public static final AnalogInputDomainConfig.AnalogDomain CURRENT
public static final AnalogInputDomainConfig.AnalogDomain VOLTAGE
public static AnalogInputDomainConfig.AnalogDomain[] values()
for (AnalogInputDomainConfig.AnalogDomain c : AnalogInputDomainConfig.AnalogDomain.values()) System.out.println(c);
public static AnalogInputDomainConfig.AnalogDomain valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2019. All rights reserved.