@ProviderType
public interface GripperCapabilities
| Modifier and Type | Method and Description |
|---|---|
GripForceCapability |
registerGrippingForceCapability(double minForce,
double maxForce,
double defaultGripForce,
Force.Unit unit)
Register a force capability for a gripper that supports gripping using a user configurable force.
|
GripVacuumCapability |
registerGrippingVacuumCapability(double minVacuum,
double maxVacuum,
double defaultGripVacuum,
Pressure.Unit unit)
Register a vacuum capability for a gripper that supports gripping using a user configurable vacuum level.
|
MultiGripperCapability |
registerMultiGripperCapability(GripperListProvider gripperListProvider)
Register a multi-gripper capability for a gripper that supports a set of multiple individual grippers/zones (from
which the end user can select an individual gripper/zone to operate).
|
SpeedCapability |
registerSpeedCapability(double minSpeed,
double maxSpeed,
double defaultGripSpeed,
double defaultReleaseSpeed,
Speed.Unit unit)
Register a speed capability for a gripper that supports operating using a user configurable speed.
|
WidthCapability |
registerWidthCapability(double minWidth,
double maxWidth,
double defaultGripWidth,
double defaultReleaseWidth,
Length.Unit unit)
Register a width/position capability for a gripper that supports moving to a user configurable position (open/close
to a configurable width).
|
WidthCapability registerWidthCapability(double minWidth, double maxWidth, double defaultGripWidth, double defaultReleaseWidth, Length.Unit unit)
minWidth - The minimum width supported by the grippermaxWidth - The maximum width supported by the gripperdefaultGripWidth - default value for the width for a grip action. This value is used for, e.g. performing a
"default" grip action using the toolbardefaultReleaseWidth - default value for the width for a release action. This value is used for, e.g. performing
a "default" release action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minWidth > maxWidthInvalidCapabilityRange - if defaultGripWidth or defaultReleaseWidth is outside the range
defined by minWidth and maxWidth.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time by a URCap implementing
the GripperContribution interface, i.e. called outside the scope of the configuration of the
gripper.CalledOutsideMethodScope - if this method is called at the wrong time by a (regular) URCap which has
registered its program node contribution/service as conformant with a PolyScope gripper (using
GripperRegistrationManager.registerAsGripper(Class)), i.e. called outside the scope of the call to
either SwingProgramNodeService.configureContribution(ContributionConfiguration) (for a Swing-based
URCap) or ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration) (for
a HTML-based URCap).GripForceCapability registerGrippingForceCapability(double minForce, double maxForce, double defaultGripForce, Force.Unit unit)
minForce - minimum force supported by the grippermaxForce - maximum force supported by the gripperdefaultGripForce - default value for the force for a grip action. This value is used for, e.g. performing a
"default" grip action using the toolbarunit - the unit for all specified values, nullInvalidCapabilityRange - if minForce > maxForce or defaultGripForce is outside the
range defined by minForce and maxForce.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time by a URCap implementing
the GripperContribution interface, i.e. called outside the scope of the configuration of the
gripper.CalledOutsideMethodScope - if this method is called at the wrong time by a (regular) URCap which has
registered its program node contribution/service as conformant with a PolyScope gripper (using
GripperRegistrationManager.registerAsGripper(Class)), i.e. called outside the scope of the call to
either SwingProgramNodeService.configureContribution(ContributionConfiguration) (for a Swing-based
URCap) or ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration) (for
a HTML-based URCap).SpeedCapability registerSpeedCapability(double minSpeed, double maxSpeed, double defaultGripSpeed, double defaultReleaseSpeed, Speed.Unit unit)
minSpeed - minimum speed supported by the grippermaxSpeed - maximum speed supported by the gripperdefaultGripSpeed - default value for the speed for a grip action. This value is used for, e.g. performing a
"default" grip action using the toolbardefaultReleaseSpeed - default value for the speed for a grip action. This value is used for, e.g. performing a
"default" release action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minSpeed > maxSpeedInvalidCapabilityRange - if defaultGripSpeed or defaultReleaseSpeed is outside the range
defined by minSpeed and maxSpeed.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time by a URCap implementing
the GripperContribution interface, i.e. called outside the scope of the configuration of the
gripper.CalledOutsideMethodScope - if this method is called at the wrong time by a (regular) URCap which has
registered its program node contribution/service as conformant with a PolyScope gripper (using
GripperRegistrationManager.registerAsGripper(Class)), i.e. called outside the scope of the call to
either SwingProgramNodeService.configureContribution(ContributionConfiguration) (for a Swing-based
URCap) or ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration) (for
a HTML-based URCap).GripVacuumCapability registerGrippingVacuumCapability(double minVacuum, double maxVacuum, double defaultGripVacuum, Pressure.Unit unit)
Register a vacuum capability for a gripper that supports gripping using a user configurable vacuum level.
If the gripper works with absolute pressure, specify a positive range for the supported vacuum level. If the gripper works with relative pressure (vacuum), specify a negative range for the supported vacuum level.minVacuum - minimum vacuum level supported by the grippermaxVacuum - maximum vacuum level supported by the gripperdefaultGripVacuum - default value for the vacuum level for a grip action. This value is used for, e.g.
performing a "default" grip action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minVacuum > maxVacuum or defaultGripVacuum is outside the
range defined by minVacuum and maxVacuum.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time by a URCap implementing
the GripperContribution interface, i.e. called outside the scope of the configuration of the
gripper.CalledOutsideMethodScope - if this method is called at the wrong time by a (regular) URCap which has
registered its program node contribution/service as conformant with a PolyScope gripper (using
GripperRegistrationManager.registerAsGripper(Class)), i.e. called outside the scope of the call to
either SwingProgramNodeService.configureContribution(ContributionConfiguration) (for a Swing-based
URCap) or ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration) (for
a HTML-based URCap).MultiGripperCapability registerMultiGripperCapability(GripperListProvider gripperListProvider)
Register a multi-gripper capability for a gripper that supports a set of multiple individual grippers/zones (from which the end user can select an individual gripper/zone to operate).
When this capability is registered, it is possible to support two use cases:
Each of the individual grippers will have to support any other capability (e.g. the width capability) that has
been registered with this interface, i.e. all the grippers will have the exact same set of capabilities. Note
that it is a requirement for registering this capability that the grippers are identical in terms of their
capabilities.
It possible to dynamically adjust properties (including the value range and default values) of each registered
capability exclusively for each individual gripper (independently of the other grippers). This is typically not
applicable for most grippers, but can be relevant when the range depends on another custom gripper setting (which
can be configured by the user).
If an update of the properties of a capability needs to apply for all individual grippers, it is more convenient
to perform the adjustment simultaneously for all grippers using the capability instance (e.g. WidthCapability)
returned when the capability was registered (with this interface).
When this capability is registered, all potentially supported grippers must be added upfront, but can be
created in an initial disabled state, and the full list of grippers must contain at least two grippers.
Adding additional grippers at a later time is not possible.
It is, however, possible to enable and disable each gripper dynamically using
MultiGripperCapability.setEnabled(SelectableGripper, boolean). This is useful, if the gripper URCap is
meant to support both a use case with only a single gripper as well as supporting the option of mounting several
separate, identical grippers on the robot at the same time. In this case, the secondary gripper(s) can be created
in an initial disabled state, and then enabled when the end user is using a multi-gripper setup.
Other contributions (for example contributed by other 3rd party URCaps) will be able to select a specific
individual gripper when creating a configuration for a GripperNode which is using this multi-gripper
device.
GripperContribution interface:
SystemConfiguration.getTCPConfiguration(SelectableGripper) method (accessible through the
systemConfiguration parameter when
GripperContribution.configureInstallation(CustomUserInputConfiguration, SystemConfiguration, TCPConfiguration, GripperAPIProvider)
is called)
gripperListProvider - Provider of the list of all supported individual grippers/zones, not null. The
implementation of GripperListProvider.getGripperList(GripperListBuilder, Locale)
will be called once (by PolyScope) to retrieve the list.CapabilityAlreadyRegistered - if this capability has already been registeredLessThanTwoGrippers - if null is returned (instead of a list) when PolyScope calls the implementation
of GripperListProvider.getGripperList(GripperListBuilder, Locale).CalledOutsideGripperConfigurationPhase - if this method is called at the wrong time by a URCap implementing
the GripperContribution interface, i.e. called outside the scope of the configuration of the
gripper.CalledOutsideMethodScope - if this method is called at the wrong time by a (regular) URCap which has
registered its program node contribution/service as conformant with a PolyScope gripper (using
GripperRegistrationManager.registerAsGripper(Class)), i.e. called outside the scope of the call to
either SwingProgramNodeService.configureContribution(ContributionConfiguration) (for a Swing-based
URCap) or ProgramNodeServiceConfigurable.configureContribution(ProgramNodeConfiguration) (for
a HTML-based URCap).Copyright © 2020. All rights reserved.