public static enum Force.Unit extends Enum<Force.Unit>
| Enum Constant and Description |
|---|
LBF
Pound-force [lbf] imperial unit.
|
N
Newton [N] SI unit.
|
| Modifier and Type | Method and Description |
|---|---|
static Force.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Force.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Force.Unit N
public static final Force.Unit LBF
public static Force.Unit[] values()
for (Force.Unit c : Force.Unit.values()) System.out.println(c);
public static Force.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.