public class LessThanTwoGrippers extends RuntimeException
GripperListBuilder.buildList(), if an attempt is made to build the list of
individual grippers/zones when less than two grippers/zones have been added. It is also thrown by
GripperCapabilities.registerMultiGripperCapability(GripperListProvider), if null is
returned by the implementation of GripperListProvider.getGripperList(GripperListBuilder, Locale).| Constructor and Description |
|---|
LessThanTwoGrippers(String message) |
addSuppressed, fillInStackTrace, getCause, getLocalizedMessage, getMessage, getStackTrace, getSuppressed, initCause, printStackTrace, printStackTrace, printStackTrace, setStackTrace, toStringpublic LessThanTwoGrippers(String message)
Copyright © 2020. All rights reserved.