| Interface | Description |
|---|---|
| GripDetectedParameters |
This interface provides parameters relevant for generating script code for the Grip Detected feedback capability
(registered using
GripperFeedbackCapabilities.registerGripDetectedCapability(ScriptCodeGenerator)). |
| GripForceCapability |
This interface represents a registered force capability for a gripper which supports gripping using a user configurable
force.
|
| GripperCapabilities |
Register the physical capabilities of the gripper using this interface.
|
| GripperFeedbackCapabilities |
Register the feedback capabilities of the gripper using this interface.
|
| GripVacuumCapability |
This interface represents a registered vacuum capability for a gripper which supports gripping using a user configurable
vacuum level.
|
| MultiGripperCapability |
This interface represents a registered multi-gripper capability for a gripper which supports multiple individual
grippers/zones.
|
| ReleaseDetectedParameters |
This interface provides parameters relevant for generating script code for the Release Detected feedback capability
(registered using
GripperFeedbackCapabilities.registerReleaseDetectedCapability(ScriptCodeGenerator)). |
| SpeedCapability |
This interface represents a registered speed capability for a gripper which supports operating using a user
configurable speed.
|
| WidthCapability |
This interface represents a registered width/position capability for a gripper which supports moving to a user
configurable position (open/close to a configurable width).
|
| Exception | Description |
|---|---|
| CapabilityAlreadyRegistered |
This exception is thrown when an attempt is made to register a capability that has already been registered.
|
| InvalidCapabilityRange |
This exception is thrown if an invalid value range or default value is specified when an attempt is made to register
a gripper capability.
|
Copyright © 2020. All rights reserved.