| Class and Description |
|---|
| SetNodeConfig |
| SetNodeConfigFactory
The SetNodeConfigFactory can be used to construct configurations that can be set on a SetNode.
|
| Class and Description |
|---|
| AnalogOutputCurrentSetNodeConfig |
| AnalogOutputSelection |
| AnalogOutputSelection.SelectionType |
| AnalogOutputVoltageSetNodeConfig |
| DigitalOutputSelection |
| DigitalOutputSelection.SelectionType |
| DigitalOutputSetNodeConfig |
| ExpressionOutputSelection |
| ExpressionOutputSelection.SelectionType |
| ExpressionOutputSetNodeConfig |
| FloatRegisterOutputSelection |
| FloatRegisterOutputSelection.SelectionType |
| FloatRegisterOutputSetNodeConfig |
| SetNodeConfig |
| SetNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2018. All rights reserved.