| Interface | Description |
|---|---|
| AnalogOutput | |
| AnalogOutputCurrentSetNodeConfig | |
| AnalogOutputSelection | |
| AnalogOutputVoltageSetNodeConfig | |
| DigitalOutput | |
| DigitalOutputSelection | |
| DigitalOutputSetNodeConfig | |
| ExpressionOutput | |
| ExpressionOutputSelection | |
| ExpressionOutputSetNodeConfig | |
| FloatRegisterOutput | |
| FloatRegisterOutputSelection | |
| FloatRegisterOutputSetNodeConfig | |
| SetNodeConfig | |
| SetNodeConfigFactory |
The SetNodeConfigFactory can be used to construct configurations that can be set on a SetNode.
|
| Enum | Description |
|---|---|
| AnalogOutputSelection.SelectionType | |
| DigitalOutputSelection.SelectionType | |
| ExpressionOutputSelection.SelectionType | |
| FloatRegisterOutputSelection.SelectionType | |
| SetNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2018. All rights reserved.