public interface ProgramNodeFactory
| Modifier and Type | Method and Description |
|---|---|
AssignmentNode |
createAssignmentNode() |
CircleMoveNode |
createCircleMoveNode() |
CommentNode |
createCommentNode() |
ElseIfNode |
createElseIfNode() |
ElseNode |
createElseNode() |
FolderNode |
createFolderNode() |
ForceNode |
createForceNode() |
HaltNode |
createHaltNode() |
IfNode |
createIfNode() |
LoopNode |
createLoopNode() |
MoveNode |
createMoveNode() |
PalletNode |
createPalletNode() |
PopupNode |
createPopupNode() |
SeekNode |
createSeekNode() |
SetNode |
createSetNode() |
URCapProgramNode |
createURCapProgramNode(Class<? extends URCapProgramNodeService> urcapProgramNodeService)
This method creates a URCap Program Node which is an instance of a
ProgramNodeContribution |
WaitNode |
createWaitNode() |
WaypointNode |
createWaypointNode() |
URCapProgramNode createURCapProgramNode(Class<? extends URCapProgramNodeService> urcapProgramNodeService)
This method creates a URCap Program Node which is an instance of a
ProgramNodeContribution
urcapProgramNodeService - is the service creating the program node contribution.URCapProgramNode which represents the ProgramNodeContribution
created by URCapProgramNodeService. Returns null if URCap providing urcapProgramNodeService is not installed.IllegalArgumentException - if the argument urcapProgramNodeService is null or urcapProgramNodeService
does not implement URCapProgramNodeServiceMoveNode createMoveNode()
WaypointNode createWaypointNode()
WaitNode createWaitNode()
SetNode createSetNode()
PopupNode createPopupNode()
HaltNode createHaltNode()
CommentNode createCommentNode()
FolderNode createFolderNode()
LoopNode createLoopNode()
AssignmentNode createAssignmentNode()
IfNode createIfNode()
ElseIfNode createElseIfNode()
ElseNode createElseNode()
CircleMoveNode createCircleMoveNode()
PalletNode createPalletNode()
SeekNode createSeekNode()
ForceNode createForceNode()
Copyright © 2018. All rights reserved.