| Interface | Description |
|---|---|
| CustomPayloadParameters |
This interface represents a configuration of the payload setting for a Gripper node where custom payload parameters
are used.
|
| GripActionConfig |
This interface represents a Gripper node configuration for a grip action.
|
| GripActionConfigBuilder |
This interface can be used to build a single gripper configuration for a grip action.
|
| GripperNodeConfig |
This base interface represents a configuration of a Gripper program node (i.e.
|
| PayloadSelection |
This interface represents a configuration of the payload setting for a Gripper node where a payload (from the
installation) has been selected.
|
| PayloadSetting |
This interface represents the configuration of the payload setting for a gripper node.
|
| ReleaseActionConfig |
This interface represents a Gripper node configuration for a release action.
|
| ReleaseActionConfigBuilder |
This interface can be used to build a single gripper configuration for a release action.
|
| SelectableGripper |
This interface represents an individual gripper in a multi-gripper device, i.e.
|
| UndefinedActionConfig |
This interface represents a Gripper node configuration where the gripper action (i.e.
|
| Enum | Description |
|---|---|
| GripperNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
| PayloadSetting.SettingType |
The setting type used to determine which type of setting this instance is.
|
Copyright © 2021. All rights reserved.