@ProviderType public interface ReleaseActionConfig extends GripperNodeConfig
GripperNodeConfig.ConfigType| Modifier and Type | Method and Description |
|---|---|
Optional<SelectableGripper> |
getGripperSelection()
This method returns the individual gripper selected (if any is selected) in a Gripper node that uses a
multi-gripper device, i.e.
|
Optional<PayloadSetting> |
getPayloadSetting()
This method returns the configuration of the payload setting for a Gripper node.
|
boolean |
isForMultiGripper()
Determine if this configuration is a multi-gripper configuration.
|
getConfigTypeboolean isForMultiGripper()
Determine if this configuration is a multi-gripper configuration. This will be the case, if the config was created
for, or retrieved from, a Gripper node that uses a multi-gripper device, i.e. a gripper device supporting the
multi-gripper capability (see the MultiGripperSupport interface).
getGripperSelection() method can be used to retrieve a (valid) gripper selection (which can be
empty). Note that, if calling the Optional.isPresent() method on the retrieved Optional
instance returns false, it can both indicate that the configuration is for a single gripper (not
supporting the multi-gripper capability) as well as indicate that no gripper has been selected (an empty
gripper selection).
true if this configuration is a multi-gripper configuration, otherwise falseOptional<SelectableGripper> getGripperSelection()
This method returns the individual gripper selected (if any is selected) in a Gripper node that uses a
multi-gripper device, i.e. a gripper device supporting the multi-gripper capability (see the
MultiGripperSupport interface).
isForMultiGripper() method can be used to determine, if this configuration is for a multi-gripper device.Optional. Use Optional.isPresent() to check,
if a gripper has been selected. The gripper selection can be retrieved using Optional.get(). Note
that Optional.isPresent() will also return false, if this configuration was created for a
single gripper. isForMultiGripper() can be used to check if this configuration is for a
multi-gripper device.Optional<PayloadSetting> getPayloadSetting()
This method returns the configuration of the payload setting for a Gripper node.
It is not mandatory to configure the Gripper node to apply a payload after the release action has finished executing and the payload setting can thus be disabled/enabled. The configuration of the payload setting will not be available here if the payload setting is disabled in the Gripper node. Therefore the returned payload setting is wrapped in anOptional, whose Optional.isPresent() method must always be used to check if the
payload setting is enabled before accessing it using Optional.get().Optional. Use Optional.isPresent() to check, if the
payload setting is enabled (since this is an optional setting). The payload setting can then be retrieved
using Optional.get().Copyright © 2021. All rights reserved.