public static enum PayloadSetting.SettingType extends Enum<PayloadSetting.SettingType>
Enum Constant and Description |
---|
CUSTOM_PARAMETERS
Custom payload parameters are specified.
|
PAYLOAD_SELECTION
A payload (from the installation) is selected.
|
UNDEFINED
No selection has been made.
|
Modifier and Type | Method and Description |
---|---|
static PayloadSetting.SettingType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static PayloadSetting.SettingType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final PayloadSetting.SettingType UNDEFINED
No selection has been made.
public static final PayloadSetting.SettingType PAYLOAD_SELECTION
A payload (from the installation) is selected.
The setting instance can be cast toPayloadSelection
.public static final PayloadSetting.SettingType CUSTOM_PARAMETERS
Custom payload parameters are specified.
The setting instance can be cast toCustomPayloadParameters
.public static PayloadSetting.SettingType[] values()
for (PayloadSetting.SettingType c : PayloadSetting.SettingType.values()) System.out.println(c);
public static PayloadSetting.SettingType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2021. All rights reserved.