public interface GripperCapabilities
| Modifier and Type | Method and Description |
|---|---|
GripForceCapability |
registerGrippingForceCapability(double minForce,
double maxForce,
double defaultGripForce,
Force.Unit unit)
Register a force capability for a gripper that supports gripping using a user configurable force.
|
GripVacuumCapability |
registerGrippingVacuumCapability(double minVacuum,
double maxVacuum,
double defaultGripVacuum,
Pressure.Unit unit)
Register a vacuum capability for a gripper that supports gripping using a user configurable vacuum level.
|
SpeedCapability |
registerSpeedCapability(double minSpeed,
double maxSpeed,
double defaultGripSpeed,
double defaultReleaseSpeed,
Speed.Unit unit)
Register a speed capability for a gripper that supports operating using a user configurable speed.
|
WidthCapability |
registerWidthCapability(double minWidth,
double maxWidth,
double defaultGripWidth,
double defaultReleaseWidth,
Length.Unit unit)
Register a width/position capability for a gripper that supports moving to a user configurable position (open/close
to a configurable width).
|
WidthCapability registerWidthCapability(double minWidth, double maxWidth, double defaultGripWidth, double defaultReleaseWidth, Length.Unit unit)
minWidth - The minimum width supported by the grippermaxWidth - The maximum width supported by the gripperdefaultGripWidth - default value for the width for a grip action. This value is used for, e.g. performing a
"default" grip action using the toolbardefaultReleaseWidth - default value for the width for a release action. This value is used for, e.g. performing
a "default" release action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minWidth > maxWidthInvalidCapabilityRange - if defaultGripWidth or defaultReleaseWidth is outside the range
defined by minWidth and maxWidth.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time, i.e. outside the scope
of the GripperContribution.configureGripper(GripperConfiguration, GripperAPIProvider) method.GripForceCapability registerGrippingForceCapability(double minForce, double maxForce, double defaultGripForce, Force.Unit unit)
minForce - minimum force supported by the grippermaxForce - maximum force supported by the gripperdefaultGripForce - default value for the force for a grip action. This value is used for, e.g. performing a
"default" grip action using the toolbarunit - the unit for all specified values, nullInvalidCapabilityRange - if minForce > maxForce or defaultGripForce is outside the
range defined by minForce and maxForce.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time, i.e. outside the scope
of the GripperContribution.configureGripper(GripperConfiguration, GripperAPIProvider) method.SpeedCapability registerSpeedCapability(double minSpeed, double maxSpeed, double defaultGripSpeed, double defaultReleaseSpeed, Speed.Unit unit)
minSpeed - minimum speed supported by the grippermaxSpeed - maximum speed supported by the gripperdefaultGripSpeed - default value for the speed for a grip action. This value is used for, e.g. performing a
"default" grip action using the toolbardefaultReleaseSpeed - default value for the speed for a grip action. This value is used for, e.g. performing a
"default" release action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minSpeed > maxSpeedInvalidCapabilityRange - if defaultGripSpeed or defaultReleaseSpeed is outside the range
defined by minSpeed and maxSpeed.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time, i.e. outside the scope
of the GripperContribution.configureGripper(GripperConfiguration, GripperAPIProvider) method.GripVacuumCapability registerGrippingVacuumCapability(double minVacuum, double maxVacuum, double defaultGripVacuum, Pressure.Unit unit)
Register a vacuum capability for a gripper that supports gripping using a user configurable vacuum level.
If the gripper works with absolute pressure, specify a positive range for the supported vacuum level. If the gripper works with relative pressure (vacuum), specify a negative range for the supported vacuum level.minVacuum - minimum vacuum level supported by the grippermaxVacuum - maximum vacuum level supported by the gripperdefaultGripVacuum - default value for the vacuum level for a grip action. This value is used for, e.g.
performing a "default" grip action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minVacuum > maxVacuum or defaultGripVacuum is outside the
range defined by minVacuum and maxVacuum.CapabilityAlreadyRegistered - if this capability has already been registeredCalledOutsideGripperConfigurationPhase - if this method is called at the wrong time, i.e. outside the scope
of the GripperContribution.configureGripper(GripperConfiguration, GripperAPIProvider) method.Copyright © 2020. All rights reserved.