public interface SpeedCapability
This interface represents a registered speed capability for a gripper which supports operating using a user configurable speed.
Through this interface, it is possible to adjust the range and default values for the speed after the capability has been registered. This is typically not applicable for most grippers, but can be relevant when the range depends on another custom gripper setting (which can be configured by the user).| Modifier and Type | Method and Description | 
|---|---|
void | 
updateCapability(double minSpeed,
                double maxSpeed,
                double defaultGripSpeed,
                double defaultReleaseSpeed,
                Speed.Unit unit)
 Update the range and default values for the speed supported by the gripper. 
 | 
void updateCapability(double minSpeed,
                      double maxSpeed,
                      double defaultGripSpeed,
                      double defaultReleaseSpeed,
                      Speed.Unit unit)
Update the range and default values for the speed supported by the gripper.
Updating the range could result in an already entered value in the configuration of a gripper program node being outside the range. This will make the given program node undefined, and force the end user to adjust the value to be valid again.minSpeed - minimum operating speed supported by the grippermaxSpeed - maximum operating speed supported by the gripperdefaultGripSpeed - default value for the speed for a grip action. This value is used for, e.g. performing a
                              "default" grip action using the toolbardefaultReleaseSpeed - default value for the speed for a release action. This value is used for, e.g. performing
                            a "default" release action using the toolbarunit - the unit for all specified values, not nullInvalidCapabilityRange - if minSpeed > maxSpeedInvalidCapabilityRange - if defaultGripSpeed or defaultReleaseSpeed is outside the range
 defined by minSpeed and maxSpeed.Copyright © 2020. All rights reserved.