public interface BlendParameters
| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
BlendParameters.ParameterType
Blend Parameters can be of different types
 The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations) 
 | 
| Modifier and Type | Method and Description | 
|---|---|
BlendParameters.ParameterType | 
getType()  | 
BlendParameters.ParameterType getType()
Copyright © 2019. All rights reserved.