| Class and Description | 
|---|
| MoveNodeConfig | 
| MoveNodeConfigFactory
 Deprecated. 
 
Use the configuration builders available in  
MoveNodeConfigBuilders interface which is accessible
 through MoveNode.getConfigBuilders(). | 
| TCPSelectionFactory
 This interface supplies methods for creating TCP selections for a Move node configuration. 
 | 
| Class and Description | 
|---|
| FeatureSelection | 
| FeatureSelection.SelectionType | 
| MoveJMotionParameters | 
| MoveJMoveNodeConfig | 
| MoveLMotionParameters | 
| MoveLMoveNodeConfig | 
| MoveNodeConfig | 
| MoveNodeConfig.ConfigType
 The configuration type used to determine which type of configuration this instance is. 
 | 
| MoveNodeTCP | 
| MovePMotionParameters | 
| MovePMoveNodeConfig | 
| TCPSelection | 
| TCPSelection.SelectionType | 
Copyright © 2019. All rights reserved.