| Interface | Description | 
|---|---|
| AssignmentNode | |
| CircleMoveNode | |
| CommentNode | |
| DirectionNode | |
| ElseIfNode | |
| ElseNode | |
| FolderNode | |
| ForceNode | |
| HaltNode | |
| IfNode | |
| LoopNode | |
| MoveNode | |
| PalletNode | |
| PopupNode | |
| SeekNode | |
| SetNode | |
| UntilNode | 
 
 The Until node is a type of program node that must be under a Waypoint node or Direction node. 
 | 
| WaitNode | |
| WaypointNode | 
| Enum | Description | 
|---|---|
| PopupNode.Type | 
| Exception | Description | 
|---|---|
| IllegalWaypointNameException | 
 This exception is thrown if trying to name a waypoint using an illegal name. 
 | 
| InvalidDomainException | 
 This exception is thrown if trying to apply an analog input/output configuration using Voltage to an IO configured to Current
 or vice versa. 
 | 
Copyright © 2019. All rights reserved.