public static enum DigitalOutputSelection.SelectionType extends Enum<DigitalOutputSelection.SelectionType>
Enum Constant and Description |
---|
DIGITAL_OUTPUT
Digital output is selected.
|
NO_DIGITAL_OUTPUT
No digital output is selected.
|
UNRESOLVED_DIGITAL_OUTPUT
The selected digital output is no longer available (e.g.
|
Modifier and Type | Method and Description |
---|---|
static DigitalOutputSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static DigitalOutputSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final DigitalOutputSelection.SelectionType NO_DIGITAL_OUTPUT
public static final DigitalOutputSelection.SelectionType UNRESOLVED_DIGITAL_OUTPUT
public static final DigitalOutputSelection.SelectionType DIGITAL_OUTPUT
DigitalOutput
public static DigitalOutputSelection.SelectionType[] values()
for (DigitalOutputSelection.SelectionType c : DigitalOutputSelection.SelectionType.values()) System.out.println(c);
public static DigitalOutputSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2018. All rights reserved.