public interface NonUserInsertable
ProgramNodeService.
If an implementation of ProgramNodeService also implements NonUserInsertable the ProgramNodeContribution
offered by the given service will not appear on the URCap sub tab of the Program tab in PolyScope,
and can not be inserted in the program tree by the end user. It can only be inserted programmatically
using the ProgramNodeFactory. This also means, it can not be inserted
using copy/paste of that node directly. It can however be inserted by copy/paste of an ancestor of such a node.Copyright © 2018. All rights reserved.