| Interface | Description |
|---|---|
| AnalogInputDomainConfig |
This interface represents the analog input domain configuration for the two analog inputs in the Tool I/O Interface.
|
| AnalogInputModeConfig |
This interface represents a configuration of the analog inputs in the Tool I/O Interface.
|
| CommunicationInterfaceConfig |
This interface represents the Tool Communication Interface (TCI) configuration for the two analog inputs in the Tool
I/O Interface.
|
| DigitalOutputModeConfig |
This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface.
|
| StandardDigitalOutputModeConfig |
This interface represents the digital output mode configuration for the digital outputs in the Tool I/O Interface.
|
| ToolIOInterface |
This interface allows for querying the settings of the Tool I/O Interface
|
| Enum | Description |
|---|---|
| AnalogInputDomainConfig.AnalogDomain |
The type of the electrical domain used by the analog inputs in the connector in the robot tool
|
| AnalogInputModeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
| CommunicationInterfaceConfig.BaudRate |
Available options for the baud rate used for communication
|
| CommunicationInterfaceConfig.Parity |
Available options for the parity used for communication
|
| CommunicationInterfaceConfig.StopBits |
Available options for the number of stop bits used for communication
|
| DigitalOutputModeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
| StandardDigitalOutputModeConfig.OutputMode |
Available output modes for the digital outputs in the connector in the robot tool.
|
| ToolIOInterface.OutputVoltage |
Available options for the output voltage level for the power supply that delivers power to the connector in the
robot tool
|
Copyright © 2021. All rights reserved.