public static enum AnalogInputDomainConfig.AnalogDomain extends Enum<AnalogInputDomainConfig.AnalogDomain>
| Enum Constant and Description |
|---|
CURRENT
Analog input configured for electric current.
|
VOLTAGE
Analog input configured for voltage.
|
| Modifier and Type | Method and Description |
|---|---|
static AnalogInputDomainConfig.AnalogDomain |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AnalogInputDomainConfig.AnalogDomain[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AnalogInputDomainConfig.AnalogDomain CURRENT
public static final AnalogInputDomainConfig.AnalogDomain VOLTAGE
public static AnalogInputDomainConfig.AnalogDomain[] values()
for (AnalogInputDomainConfig.AnalogDomain c : AnalogInputDomainConfig.AnalogDomain.values()) System.out.println(c);
public static AnalogInputDomainConfig.AnalogDomain valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2021. All rights reserved.