| Class and Description |
|---|
| ScrewdriverCapabilities
Register the capabilities of the screwdriver using this interface.
|
| ScrewdriverFeedbackCapabilities
Register the feedback capabilities of the screwdriver using this interface.
|
| Class and Description |
|---|
| DriveScrewNotOKParameters
This interface provides parameters relevant for generating script code for the Drive Screw Not OK feedback capability
(registered using
ScrewdriverFeedbackCapabilities.registerDriveScrewNotOKCapability(ScriptCodeGenerator)). |
| DriveScrewOKParameters
This interface provides parameters relevant for generating script code for the Drive Screw OK feedback capability
(registered using
ScrewdriverFeedbackCapabilities.registerDriveScrewOKCapability(ScriptCodeGenerator)). |
| FeedScrewParameters
This interface provides parameters relevant for generating script code for the Feed Screw capability
(registered using
ScrewdriverCapabilities.registerFeedScrewCapability(ScriptCodeGenerator)). |
| PrepareToStartScrewdriverParameters
This interface provides parameters relevant for generating script code for the Prepare To Start Screwdriver capability
(registered using
ScrewdriverCapabilities.registerPrepareToStartScrewdriverCapability(ScriptCodeGenerator)). |
| ProgramSelectionParameters
This interface provides parameters relevant for generating script code for the Program Selection capability
(registered using
ScrewdriverCapabilities.registerProgramSelectionCapability(ScrewdriverProgramListProvider, ScriptCodeGenerator)). |
| ScrewdriverReadyParameters
This interface provides the parameters relevant for generating script for the Screwdriver Ready feedback operation
capability (registered using
ScrewdriverFeedbackCapabilities.registerScrewdriverReadyCapability(ScriptCodeGenerator)). |
Copyright © 2021. All rights reserved.