| Interface | Description |
|---|---|
| ContributionConfiguration |
Provides access to configure optional PolyScope properties of a screwdriver contribution.
|
| ScrewdriverAPIProvider |
This interface provides access to functionality and services available from within PolyScope relevant for screwdriver
contributions.
|
| ScrewdriverConfiguration |
This interface provides access to register or setup various properties and capabilities of a screwdriver.
|
| ScrewdriverContribution |
This interface defines an API for adding functionality for screwdrivers to PolyScope.
|
| ScrewdriverParameters |
This interface represents parameters for a screwdriver operation defined/configured by the end user.
|
| SystemConfiguration |
This interface provides access to functionality for configuring the robot system (separate from the screwdriver),
e.g.
|
| Enum | Description |
|---|---|
| ScrewdriverOperationType |
This interface represents the type of screwing operation performed by the screwdriver.
|
| Exception | Description |
|---|---|
| CalledOutsideScrewdriverConfigurationPhase |
This exception is thrown if an attempt is made to register a capability outside the scope of the Screwdriver Configuration
phase, i.e.
|
Copyright © 2021. All rights reserved.