public interface StandardDigitalOutputModeConfig extends DigitalOutputModeConfig
This interface represents the digital output mode configuration for the digital outputs in the Tool I/O Interface.
 To create a new configuration, see the DigitalOutputModeConfigFactory interface which is accessible through
 ToolIOInterfaceControllable.getDigitalOutputModeConfigFactory(). 
 To apply a configuration, see ToolIOInterfaceControllable.setDigitalOutputModeConfig(DigitalOutputModeConfig).
 
| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
StandardDigitalOutputModeConfig.OutputMode
Available output modes for the digital outputs in the connector in the robot tool. 
 | 
DigitalOutputModeConfig.ConfigType| Modifier and Type | Method and Description | 
|---|---|
StandardDigitalOutputModeConfig.OutputMode | 
getOutputModeForOutput0()  | 
StandardDigitalOutputModeConfig.OutputMode | 
getOutputModeForOutput1()  | 
getConfigTypeStandardDigitalOutputModeConfig.OutputMode getOutputModeForOutput0()
StandardDigitalOutputModeConfig.OutputMode getOutputModeForOutput1()
Copyright © 2020. All rights reserved.