public interface AnalogInputUntilNodeConfig extends IOInputUntilNodeConfig
| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
AnalogInputUntilNodeConfig.InputDomainType
The type of the electrical domain used by an analog input. 
 | 
IOInputUntilNodeConfig.SelectionTypeUntilNodeConfig.ConfigType| Modifier and Type | Method and Description | 
|---|---|
CompareOperator | 
getCompareOperator()  | 
Current | 
getCurrentThreshold()  | 
AnalogIO | 
getInput()
 Retrieves the selected analog input used by the until condition. 
 | 
AnalogInputUntilNodeConfig.InputDomainType | 
getInputDomainType()  | 
Voltage | 
getVoltageThreshold()  | 
getTypegetConfigTypeAnalogInputUntilNodeConfig.InputDomainType getInputDomainType()
AnalogIO getInput()
Retrieves the selected analog input used by the until condition.
Note: The selected analog input might no longer be available (e.g. because a selected analog Tool input is used for Tool Communication Interface). The presence of the selected analog input can be verified usingAnalogIO.isResolvable().CompareOperator getCompareOperator()
Current getCurrentThreshold()
IllegalStateException - if the selected analog input is using the Voltage electrical domain. Use
         getInputDomainType() to determine the electrical domain type used by the selected analog input.Voltage getVoltageThreshold()
IllegalStateException - if the selected analog input is using the Current electrical domain. Use
         getInputDomainType() to determine the electrical domain type used by the selected analog input.Copyright © 2020. All rights reserved.