public static enum AnalogInputUntilNodeConfig.InputDomainType extends Enum<AnalogInputUntilNodeConfig.InputDomainType>
Enum Constant and Description |
---|
CURRENT
The selected electrical domain for the analog input is Current.
|
VOLTAGE
The selected electrical domain for the analog input is Voltage.
|
Modifier and Type | Method and Description |
---|---|
static AnalogInputUntilNodeConfig.InputDomainType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AnalogInputUntilNodeConfig.InputDomainType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AnalogInputUntilNodeConfig.InputDomainType CURRENT
public static final AnalogInputUntilNodeConfig.InputDomainType VOLTAGE
public static AnalogInputUntilNodeConfig.InputDomainType[] values()
for (AnalogInputUntilNodeConfig.InputDomainType c : AnalogInputUntilNodeConfig.InputDomainType.values()) System.out.println(c);
public static AnalogInputUntilNodeConfig.InputDomainType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.