public static enum IOInputUntilNodeConfig.SelectionType extends Enum<IOInputUntilNodeConfig.SelectionType>
Enum Constant and Description |
---|
ANALOG_INPUT
Analog input is selected.
|
DIGITAL_INPUT
Digital input is selected.
|
FLOAT_REGISTER_INPUT
A float input register is selected.
|
NONE
The node is not fully configured.
|
Modifier and Type | Method and Description |
---|---|
static IOInputUntilNodeConfig.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static IOInputUntilNodeConfig.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final IOInputUntilNodeConfig.SelectionType NONE
public static final IOInputUntilNodeConfig.SelectionType DIGITAL_INPUT
Digital input is selected.
The config instance can be cast toDigitalInputUntilNodeConfig
.public static final IOInputUntilNodeConfig.SelectionType ANALOG_INPUT
Analog input is selected.
The config instance can be cast toAnalogInputUntilNodeConfig
.public static final IOInputUntilNodeConfig.SelectionType FLOAT_REGISTER_INPUT
A float input register is selected.
The config instance can be cast toFloatRegisterInputUntilNodeConfig
.public static IOInputUntilNodeConfig.SelectionType[] values()
for (IOInputUntilNodeConfig.SelectionType c : IOInputUntilNodeConfig.SelectionType.values()) System.out.println(c);
public static IOInputUntilNodeConfig.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.