public interface IO
| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
IO.InterfaceType  | 
static class  | 
IO.IOType  | 
| Modifier and Type | Method and Description | 
|---|---|
String | 
getDefaultName()  | 
IO.InterfaceType | 
getInterfaceType()  | 
String | 
getName()  | 
IO.IOType | 
getType()  | 
String | 
getValueStr()  | 
boolean | 
isInput()  | 
boolean | 
isResolvable()
Some I/Os, such as MODBUS I/Os and analog Tool inputs, are in some situations not present in PolyScope or available
 for use. 
 | 
String getName()
String getDefaultName()
IO.IOType getType()
IO.InterfaceType getInterfaceType()
boolean isInput()
true if I/O supports reading of values and false otherwise.String getValueStr()
boolean isResolvable()
ModbusIO.isResolvable().true, if I/O can be resolved.
         false otherwise.Copyright © 2020. All rights reserved.