IO.InterfaceType, IO.IOType| Modifier and Type | Method and Description | 
|---|---|
boolean | 
getValue()  | 
boolean | 
isResolvable()
Some digital I/Os, such as the digital tool outputs, are in some situations not available for use. 
 | 
boolean | 
setValue(boolean high)
Set digital I/O output signal. 
 | 
getDefaultName, getInterfaceType, getName, getType, getValueStr, isInputboolean setValue(boolean high)
high - the digital value to be set.true if the digital signal was set, false if the signal was not set, e.g. because the
 controller was not running.boolean getValue()
boolean isResolvable()
isResolvable in interface IOtrue, if digital I/O can be resolved.
         false otherwise, e.g. because a tool output has been configured to Dual Pin Power.Copyright © 2020. All rights reserved.