@ProviderType
public interface ApplicationAPI
| Modifier and Type | Method and Description | 
|---|---|
<T extends DeviceManager> | 
getDeviceManager(Class<T> deviceManagerClass)
This method can be used to get a specific  
DeviceManager instance | 
FeatureModel | 
getFeatureModel()  | 
<T extends InstallationNodeContribution> | 
getInstallationNode(Class<T> installationType)
This method can be used to get a specific  
InstallationNodeContribution instance | 
IOModel | 
getIOModel()  | 
ResourceModel | 
getResourceModel()  | 
TCPModel | 
getTCPModel()  | 
ValueFactoryProvider | 
getValueFactoryProvider()  | 
VariableModel | 
getVariableModel()  | 
IOModel getIOModel()
FeatureModel getFeatureModel()
TCPModel getTCPModel()
VariableModel getVariableModel()
ResourceModel getResourceModel()
ValueFactoryProvider getValueFactoryProvider()
<T extends InstallationNodeContribution> T getInstallationNode(Class<T> installationType)
InstallationNodeContribution instanceT - The generic for specifying the InstallationNodeContributioninstallationType - The class of the installation node contribution to return<T extends DeviceManager> T getDeviceManager(Class<T> deviceManagerClass)
DeviceManager instanceT - The generic type of class to returndeviceManagerClass - The class for the device manager to returnCopyright © 2020. All rights reserved.