public interface VariableModel
DataModel instance or used for the configuration of a built-in PolyScope program node.| Modifier and Type | Method and Description | 
|---|---|
Collection<Variable> | 
get(Filter<Variable> filter)
Get a subset of all the variables registered in the system using a filter. 
 | 
Collection<Variable> | 
getAll()  | 
FeatureVariable | 
getFeatureVariable(Feature feature)
Get the feature variable for a  
Feature. | 
VariableFactory | 
getVariableFactory()  | 
Collection<Variable> getAll()
Collection<Variable> get(Filter<Variable> filter)
filter - see VariableFilterFactory for examples.VariableFactory getVariableFactory()
VariableFactory to create variable objects.FeatureVariable getFeatureVariable(Feature feature)
Feature.feature - the feature with a variable.IllegalArgumentException - If feature not is present in the installation or feature has no variable,
 see Feature.isVariable().Copyright © 2020. All rights reserved.