| Interface | Description | 
|---|---|
| DriveScrewNotOKParameters | 
 
 This interface provides parameters relevant for generating script code for the Drive Screw Not OK feedback capability
 (registered using  
ScrewdriverFeedbackCapabilities.registerDriveScrewNotOKCapability(ScriptCodeGenerator)). | 
| DriveScrewOKParameters | 
 
 This interface provides parameters relevant for generating script code for the Drive Screw OK feedback capability
 (registered using  
ScrewdriverFeedbackCapabilities.registerDriveScrewOKCapability(ScriptCodeGenerator)). | 
| FeedScrewParameters | 
 
 This interface provides parameters relevant for generating script code for the Feed Screw capability
 (registered using  
ScrewdriverCapabilities.registerFeedScrewCapability(ScriptCodeGenerator)). | 
| PrepareToStartScrewdriverParameters | 
 
 This interface provides parameters relevant for generating script code for the Prepare To Start Screwdriver capability
 (registered using  
ScrewdriverCapabilities.registerPrepareToStartScrewdriverCapability(ScriptCodeGenerator)). | 
| ProgramSelectionParameters | 
 
 This interface provides parameters relevant for generating script code for the Program Selection capability
 (registered using  
ScrewdriverCapabilities.registerProgramSelectionCapability(ScrewdriverProgramListProvider, ScriptCodeGenerator)). | 
| ScrewdriverCapabilities | 
 
 Register the capabilities of the screwdriver using this interface. 
 | 
| ScrewdriverFeedbackCapabilities | 
 
 Register the feedback capabilities of the screwdriver using this interface. 
 | 
| ScrewdriverReadyParameters | 
 This interface provides the parameters relevant for generating script for the Screwdriver Ready feedback operation
 capability (registered using  
ScrewdriverFeedbackCapabilities.registerScrewdriverReadyCapability(ScriptCodeGenerator)). | 
| Exception | Description | 
|---|---|
| CapabilityAlreadyRegistered | 
 This exception is thrown when an attempt is made to register a capability that has already been registered. 
 | 
Copyright © 2020. All rights reserved.