public interface PrepareToStartScrewdriverParameters
 This interface provides parameters relevant for generating script code for the Prepare To Start Screwdriver capability
 (registered using ScrewdriverCapabilities.registerPrepareToStartScrewdriverCapability(ScriptCodeGenerator)).
 
 These parameters are passed when PolyScope calls the implementation of the ScriptCodeGenerator.generateScript(ScriptWriter, Object)
 method responsible for the generating the script code.
 
Copyright © 2020. All rights reserved.