| Class and Description |
|---|
| ToolIOInterface
This interface allows for querying the settings of the Tool I/O Interface
|
| Class and Description |
|---|
| AnalogInputDomainConfig.AnalogDomain
The type of the electrical domain used by the analog inputs in the connector in the robot tool
|
| AnalogInputModeConfig
This interface represents a configuration of the analog inputs in the Tool I/O Interface.
|
| AnalogInputModeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
| CommunicationInterfaceConfig.BaudRate
Available options for the baud rate used for communication
|
| CommunicationInterfaceConfig.Parity
Available options for the parity used for communication
|
| CommunicationInterfaceConfig.StopBits
Available options for the number of stop bits used for communication
|
| DigitalOutputModeConfig
This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface.
|
| DigitalOutputModeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
| StandardDigitalOutputModeConfig.OutputMode
Available output modes for the digital outputs in the connector in the robot tool.
|
| ToolIOInterface.OutputVoltage
Available options for the output voltage level for the power supply that delivers power to the connector in the
robot tool
|
| Class and Description |
|---|
| AnalogInputDomainConfig
This interface represents the analog input domain configuration for the two analog inputs in the Tool I/O Interface.
|
| AnalogInputDomainConfig.AnalogDomain
The type of the electrical domain used by the analog inputs in the connector in the robot tool
|
| AnalogInputModeConfig
This interface represents a configuration of the analog inputs in the Tool I/O Interface.
|
| CommunicationInterfaceConfig
This interface represents the Tool Communication Interface (TCI) configuration for the two analog inputs in the Tool
I/O Interface.
|
| CommunicationInterfaceConfig.BaudRate
Available options for the baud rate used for communication
|
| CommunicationInterfaceConfig.Parity
Available options for the parity used for communication
|
| CommunicationInterfaceConfig.StopBits
Available options for the number of stop bits used for communication
|
| DigitalOutputModeConfig
This interface represents a configuration of the output mode for the digital outputs in the Tool I/O Interface.
|
| StandardDigitalOutputModeConfig
This interface represents the digital output mode configuration for the digital outputs in the Tool I/O Interface.
|
| StandardDigitalOutputModeConfig.OutputMode
Available output modes for the digital outputs in the connector in the robot tool.
|
| ToolIOInterface
This interface allows for querying the settings of the Tool I/O Interface
|
| ToolIOInterface.OutputVoltage
Available options for the output voltage level for the power supply that delivers power to the connector in the
robot tool
|
Copyright © 2019. All rights reserved.