| Package | Description |
|---|---|
| com.ur.urcap.api.domain.resource.tooliointerface | |
| com.ur.urcap.api.domain.resource.tooliointerface.control |
| Modifier and Type | Method and Description |
|---|---|
AnalogInputDomainConfig.AnalogDomain |
AnalogInputDomainConfig.getAnalogDomainForInput0()
This method returns the type of electrical domain used by analog input 0 in the connector in the robot tool
(labeled 'analog_in[2]' in PolyScope)
|
AnalogInputDomainConfig.AnalogDomain |
AnalogInputDomainConfig.getAnalogDomainForInput1()
This method returns the type of electrical domain used by analog input 1 in the connector in the robot tool
(labeled 'analog_in[3]' in PolyScope).
|
static AnalogInputDomainConfig.AnalogDomain |
AnalogInputDomainConfig.AnalogDomain.valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AnalogInputDomainConfig.AnalogDomain[] |
AnalogInputDomainConfig.AnalogDomain.values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
| Modifier and Type | Method and Description |
|---|---|
AnalogInputDomainConfig |
AnalogInputModeConfigFactory.createAnalogInputDomainConfig(AnalogInputDomainConfig.AnalogDomain input0,
AnalogInputDomainConfig.AnalogDomain input1)
Create a configuration to set the electrical domain of the analog inputs in the connector in the robot tool
|
Copyright © 2019. All rights reserved.