| Interface | Description |
|---|---|
| AssignmentNode | |
| CircleMoveNode | |
| CommentNode | |
| DirectionNode | |
| ElseIfNode | |
| ElseNode | |
| FolderNode | |
| ForceNode | |
| HaltNode | |
| IfNode | |
| LoopNode | |
| MoveNode | |
| PalletNode | |
| PopupNode | |
| ScrewdrivingNode | |
| SeekNode | |
| SetNode | |
| UntilNode |
The Until node is a type of program node that must be under a Waypoint node or Direction node.
|
| WaitNode | |
| WaypointNode |
| Enum | Description |
|---|---|
| PopupNode.Type |
| Exception | Description |
|---|---|
| IllegalWaypointNameException |
This exception is thrown if trying to name a waypoint using an illegal name.
|
| InvalidDomainException |
This exception is thrown if trying to apply an analog input/output configuration using Voltage to an IO configured to Current
or vice versa.
|
Copyright © 2019. All rights reserved.