public interface PopupNode extends ProgramNode
| Modifier and Type | Interface and Description |
|---|---|
static class |
PopupNode.Type |
| Modifier and Type | Method and Description |
|---|---|
String |
getMessage() |
PopupNode.Type |
getType() |
PopupNode |
setMessage(String message) |
PopupNode |
setType(PopupNode.Type type) |
PopupNode setMessage(String message)
message - the message in the pop up for the end userIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)String getMessage()
PopupNode setType(PopupNode.Type type)
type - the type of pop upIllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)PopupNode.Type getType()
Copyright © 2019. All rights reserved.