public interface MoveNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
MoveNodeConfig |
getConfig() |
MoveNodeConfigBuilders |
getConfigBuilders()
This method returns a
MoveNodeConfigBuilders to build configurations for this node type. |
MoveNodeConfigFactory |
getConfigFactory()
Deprecated.
Use
getConfigBuilders() instead. |
TCPSelectionFactory |
getTCPSelectionFactory()
This method returns a
TCPSelectionFactory to create a TCP selection. |
MoveNode |
setConfig(MoveNodeConfig config)
Set a configuration on this node.
|
@Deprecated MoveNodeConfigFactory getConfigFactory()
getConfigBuilders() instead.MoveNode setConfig(MoveNodeConfig config)
config - the configuration to be set.IllegalArgumentException - if this node is a MoveP containing one or more CircleMoveNode and the node
configuration is attempted to be changed to MoveJ or MoveL. CircleMoveNode is only allowed under a MoveP.
All instances of CircleMoveNode need to be deleted before the configuration can be changed from a MoveP to
MoveJ or MoveL.IllegalArgumentException - if this node is a MoveL or MoveP containing one or more DirectionNode and
the node configuration is attempted to be changed to a MoveJ.
DirectionNode is only allowed under a MoveL or MoveP. All instances of DirectionNode need to be
deleted before the configuration can be changed from a MoveL or MoveP to a MoveJ.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager).MoveNodeConfig getConfig()
MoveNodeConfigBuilders getConfigBuilders()
MoveNodeConfigBuilders to build configurations for this node type.TCPSelectionFactory getTCPSelectionFactory()
TCPSelectionFactory to create a TCP selection.Copyright © 2019. All rights reserved.