| Interface | Description | 
|---|---|
| FeatureSelection | |
| MoveJMotionParameters | |
| MoveJMoveNodeConfig | |
| MoveLMotionParameters | |
| MoveLMoveNodeConfig | |
| MoveNodeConfig | |
| MoveNodeConfigFactory | Deprecated Use the configuration builders available in  MoveNodeConfigBuildersinterface which is accessible
 throughMoveNode.getConfigBuilders(). | 
| MoveNodeFeature | |
| MoveNodeTCP | |
| MovePMotionParameters | |
| MovePMoveNodeConfig | |
| TCPSelection | |
| TCPSelectionFactory | This interface supplies methods for creating TCP selections for a Move node configuration. | 
| Enum | Description | 
|---|---|
| FeatureSelection.SelectionType | |
| MoveNodeConfig.ConfigType | The configuration type used to determine which type of configuration this instance is. | 
| TCPSelection.SelectionType | 
Copyright © 2019. All rights reserved.