| Interface | Description | 
|---|---|
| MoveJConfigBuilder | 
 This interface can be used to build a single MoveJ configuration that can be applied to a Move node. | 
| MoveLConfigBuilder | 
 This interface can be used to build a single MoveL configuration that can be applied to a Move node. | 
| MoveNodeConfigBuilders | This interface provides access to a set of builders which can be used to create Move node configurations
 for all the different supported move types. | 
| MovePConfigBuilder | 
 This interface can be used to build a single MoveP configuration that can be applied to a Move node. | 
Copyright © 2019. All rights reserved.