| Class and Description |
|---|
| MoveNodeConfigBuilders
This interface provides access to a set of builders which can be used to create Move node configurations
for all the different supported move types.
|
| Class and Description |
|---|
| MoveJConfigBuilder
This interface can be used to build a single MoveJ configuration that can be applied to a Move node.
|
| MoveLConfigBuilder
This interface can be used to build a single MoveL configuration that can be applied to a Move node.
|
| MovePConfigBuilder
This interface can be used to build a single MoveP configuration that can be applied to a Move node.
|
Copyright © 2019. All rights reserved.