public interface TCPContributionModel
This interface provides functionality for adding, updating and removing TCPs in PolyScope.
Note: This interface must only be used in an installation contribution.Modifier and Type | Method and Description |
---|---|
TCP |
addTCP(String idKey,
String suggestedName,
Pose offset)
Add a TCP to the current PolyScope installation.
|
TCP |
getTCP(String idKey)
Returns the TCP previously added by this URCap using the same
idKey . |
void |
removeTCP(String idKey)
Remove a TCP added by this URCap from PolyScope.
|
void |
updateTCP(String idKey,
Pose newOffset)
Update the offset of a TCP already added by this URCap.
|
TCP addTCP(String idKey, String suggestedName, Pose offset)
idKey
- The key to identify this TCP by. The key is for this URCap only, i.e. it only has to be unique for
this URCap and not "globally" for other URCaps.suggestedName
- Suggested name for the TCP. Valid names must match regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a
total of 15 characters. The final name can be retrieved from the returned TCP instance.offset
- The offset of the TCP with respect to the tool output flangeTCPAlreadyAddedException
- If called twice using the same idKey
.
Use getTCP(String)
to check if the TCP has already been added to the
current installation.
Use updateTCP(String, Pose)
to update the TCP if the offset of the TCP
has changed.IllegalTCPNameException
- If the suggested name does not match required regex.IllegalArgumentException
- If the pose specified for the offset is not inside the valid range of a TCP offset
as defined by PolyScope.TCP getTCP(String idKey)
idKey
. Use this to verify if the TCP is
present in the current installation.idKey
- The key to identify this TCP by.null
if no TCP exists in current installation.void updateTCP(String idKey, Pose newOffset)
idKey
- The key to identify the TCP. A TCP must have been added prior to this method call using the same key.newOffset
- The new offset to set for the TCP with respect to the tool output flange.TCPNotFoundException
- If no TCP exists with the provided idKey
.IllegalArgumentException
- If the pose specified for the offset is not inside the valid range of a TCP offset
as defined by PolyScope.void removeTCP(String idKey)
idKey
- The key used to add the TCP with.TCPNotFoundException
- If no TCP exists with the provided idKey
.Copyright © 2019. All rights reserved.